GEMU's websites make use of cookies. If you are using the site, this means that you agree to the use of cookies. To implement personal settings, click here

GEMÜ glossary for valves and

automation components

Our glossary provides an explanation of around 400 technical terms and abbreviations relating to the pipeline construction sector. It focuses on valves, measurement and control systems and their areas of application.

AB more
​Drugs and Medicines Register of the Federal Republic of Germany. See also Pharmakopoea.
less
Abrasion more
​​Abrasion refers to the wear mechanics between two or more substances.In mechanical design, for example, the wear mechanics occur between a moving shaft and its bearing.In flow technology, the wear mechanics take the form of a damaging interaction between a flowing medium (fluid) and a surface that comes into contact with the flowing medium (e.g. steam flows through a valve or a pump conveys sandy water). The intensity of the abrasion depends on the cybernetic energy and the particle/drip potential of a fluid as well as the properties of the medium and the surface it comes into contact with. The fundamental meaning of abrasion is very close to "shaving off".Abrasive behaviour occurs, for example, when the components of a flowing medium cannot follow the change in direction of the carrier medium quickly enough, which means that they bounce against an obstruction and transfer their dynamic energy into the obstruction (e.g. drops of liquid or solid matter within steams or gases or solid matter within liquids). If the obstruction cannot deflect or compensate for this energy, it is destroyed. There are two measures that can be implemented in order to minimize abrasive behaviour:Limit the flow velocity of the medium as far as possible (e.g. by restricting the pump power or by using larger cross-sections).Design the surfaces to be either very hard or very soft (e.g. coating with glass or rubber linings).In the case of a hard coating, the particles bounce off the surface; in the case of a soft surface the particles spring back. It is not possible to provide 100% protection against the abrasive behaviour of fluids, which means that the plant and its components must be checked regularly so that any faulty devices can be replaced in good time. Abrasion is often confused with the phenomenon of cavitation. This, however, is the pressure-/flow-dependent formation of small vapour bubbles in liquids, which, when they collapse by way of a rapid implosion, can cause material to be torn away from the surface of the stream body (e.g. in the case of propellers or in pipe bends).







less
Absolute pressure more
​Absolute pressure is pressure measured relative to zero pressure (vacuum). The reference point is pressure = 0, i.e. perfect vacuum.
less
Absorption more
This procedure describes an effect in which a substance penetrates into the core of a solid or liquid.
less
Actual value "x" more
​The actual value is the continuously determined actual, existing process variable X in a control system (e.g. stroke distance/valve position for position controls or temperature, pressure, pH value, diffusion, volumetric flow for process controls).
less
Actuator more
​An actuator is a component for switching a process, e.g. servo-motor, solenoid valve. It intervenes in the process and changes the substance or energy flows. Actuators often convert these into mechanical work, e.g. movement.
less
Adsorption more
​Adsorption is the enrichment of substances at the surface of a body or at interfaces
less
AISI more
​American Iron Steel Institute
less
AMA Fachverband für Sensorik e.V. more
​Founded in 1980 as "Arbeitsgemeinschaft Messwertaufnehmer"(consortium for measured value indicators). Represents the interests of all groups involved in the field of sensor system processes.  
less
Ambient temperature more
​Symbol: t ambient Is the prevailing temperature of the ambient atmosphere on a device (e.g. a pump or a valve). Since the ambient temperature may fluctuate the possible occasional temperature peaks must also be considered in addition to the largely prevailing ambient temperature when assessing whether a device can be used. The operating and ambient temperatures are in direct relation with the temperature resistance of a device. If the manufacturer’s specifications are insufficient for an assessment or incomplete, proceed according to the temperature formula for devices. The formula can only be used if the actual ambient temperature is above 20 °C. It must be noted, however, that the manufacturer‘ specifications have priority. It the ambient temperature is below 20 °C, the formula does not work.   Operating temp.max.safe function = (operating temp.max. manufacturer spec. + 20 °C) - ambient temp.actual


less
AMWHV more
see GMP​
less
Angle gauge more
In the context of diaphragm valve technology, this is an easy to operate angle measuring device, which is placed on the valve body in place of the actuator and is locked in place with a quick-release apparatus. The discharge angle specified by the valve manufacturer can be set on a scale. The valve is then rotated out of its vertical position until the air bubble lies in the centre of the spirit level. Angle gauges are available for diaphragm sizes MG 25/DN15-25, MG 40/DN 32+40 and MG 50/DN50 (see also Discharge angle).
less
Angle of rotation more
Applies to the field of valve installation. Alternative term for discharge angle or the angle by which a diaphragm valve needs to be rotated in the pipe axis so that the working medium can flow around the sealing weir of the valve unhindered (see Discharge angle).
less
ANSI more
​American National Standards Institute
less
APC more
​Advanced Process Control is a superior method for controlling processes. It is used to control reactors and centrifuges as well as start-up, load change and product switching processes. ApC can help to minimize energy consumption, raw material consumtion and fluctuations of a process.
less
Aqua ad injectabile (WFI) more
Water for Injection purposes. Pyrogen-free, sterile water. WFI water according to DAB must be produced by distillation. WFI water according to USP can be made by reverse osmosis combined with an ion exchange or ultra-filtration. 
less
Aqua demineralisata more
​Demineralised water See D-Water and DI Water.
less
Aqua pro injectione more
​See Aqua ad injectabile (WFI)
less
Aquapurifica more
​Purified water Made for example by distillation, ion exchange, reverse osmosis or ultra-filtration from drinking water. No direct demand for sterility in accordance with drinking water quality.
less
Aseptic more
​Germ-free See Aseptics  
less
Aseptic preparation more
​Operating technique for manufacturing and processing products which cannot be sterilised later. Avoidance of microbial contamination by combining suitable methods, e.g. the use of a sterile process technology and use of germ-free materials.
less
Aseptic process more
In an aseptic process (according to the FDA), the pharmaceutical product, the container and the closure are subjected to separate sterilization methods and then brought back together. As there is no process to sterilize the product in its final container, it is essential that containers are filled and sealed in an extremely high-quality environment.
less
Aseptics more
​Knowledge of freedom from germs, e.g. working under aseptic conditions. Originally avoidance of sepsis (blood poisoning), today the avoidance of microbial contamination both in medical applications, e.g. during operations and in the manufacture of sterile products.
less
ASME more
The American Society of Mechanical Engineers issues the BPE (Bio Processing Equipment Standard).
less
ASTM more
​American Society of Testing Materials
less
ATEX more
​Is the generally used working title/generic term for the European regulations 94/9/EC (equipment and manufacturer-oriented) and 99/92/EC (plant and owner-oriented) which are concerned with the handling of explosive environments in general (Atmospheres explosibles). In this context, national regulations concentrated in the past especially on the standardisation of electrically powered devices which was generally known under the term "EX-protection". However, other factors may also represent a source of danger. Certain materials are susceptible to dangerous static charges for example and hot surfaces may also act as ignition sources. Therefore, since 2003, the European Community has been passing laws to govern the overall assessment to protect its citizens/workers. The Directive 94/9/EC ATEX 95a (formerly 100a) exactly standardises the primary and secondary explosion protection. Primary means the avoidance, prevention or restriction of explosive atmospheres (the responsibility of the plant owner). Secondary means prevention of an explosion by using suitable technical means in the presence of ignition sources or ignitable materials (the responsibility of the equipment manufacturer). For this the danger areas (primary) are divided into zones and classified in explosion technical groups so that the prevailing danger situation can be clearly assessed and defined. To ensure the explosion protection of the planned/used devices, machines and parts (secondary) two main groups are distinguished which are defined on the one hand in the standard for electrical appliances DIN EN 50014 (and following) and on the other hand in the standard for non-electrical appliances DIN EN 13463-1. If a device, machine or single part is to be used in an explosive environment, the owner must first assess and classify the special situation. The entire equipment for this area is then procured based on this. The equipment/component providers are obliged to submit the appropriate conformity/applicability declarations if they are entitled to do so according to pertinent regulations and if the product meets requirements. The observance and implementation of other regulations and standards may be necessary for this. This always differs depending on the device (e.g. pressure equipment directive, regulations for electrical and electronic equipment, machine directive etc.).

less
Attestation for sterilisation more
​See sterile test and validation
less
Autoclave more
Generally refers to a closed room or area. In the context of sterile applications, it is a pressure vessel that can be sealed gas-tight in which, for example, products, devices, surgical instruments, valves and plant components are sterilized with a vacuum or saturated steam (see also Autoclaving). less
Autoclaving more

In the context of plant engineering, this is a sterilization process in a closed container (autoclave) in which products, plant components or devices to be sterilized are placed and completely sterilized inside and out with saturated steam. Autoclaving is always preceded by multi-stage cleaning of the devices/parts to be autoclaved. There are two basic types of autoclaving: The vacuum procedure, in which the air is pumped out of the autoclave several times, alternating with an inflow of steam, and the flow or gravitation procedure, in which the air is completely displaced by saturated steam.

less
B-value more
​Dimensionless number Value used in the food and dairy industry for determining the extermination effect in sterilisation processes. Siehe auch F-value.
less
Bacteria more
​Single-cell microscopic life forms / micro-organisms without a cell core (procaryonts) which reproduce by division. Procaryontic single-cell organisms are organisms which are distinguishable by their form, growth conditions and metabolism. The bacteria are divided into many different types and families. They can transfer diseases to humans (e.g. the bacterium borrelia burgdorferi which is transmitted by tick bites and which causes Lyme borreliosis) or may be important for a healthy bowel flora and therefore indispensable for humans (the bowel bacterium E.coli). The first molecular biology experiments and later genetic engineering experiments were made on the E.coli bacterium. The remnants of dead bacteria are often as dangerous as the bacterium itself in pharmaceutical application.
less
Bacteriology more
​Knowledge of bacteria
less
Bacteriostatic more
​Retardant to bacterial growth Bacteriostatically active materials retard or prevent bacterial growth.
less
BAM more
Federal Institute for Material Research and Testing
less
Batch more
​A product quantity produced in one or more processes which is considered homogeneous (product with identical properties).
less
BBD more
​Best before dateSee also DIN 10 503
less
Benchmarking more
​Bench marking is a method of assessing the performance of a company, for example based on predefined characteristics in order to create comparability. These benchmarks indicate strength and weaknesses in individual areas and offer the possibility of optimization. 
less
BfArM more
Federal Institute for Pharmaceutical and Medical Products
less
Biofilms more
​Biofilms are large accumulations of bacteria and other micro-organisms which are bound in a sticky mass of intertwined polysaccharide fibres which connect cells and bind them at the surface. The micro-organism contamination of materials used in watery pharmaceutical and biotechnical production systems is well documented. There would be no organically arranged tissue without biological adhesion. Biofilm contamination thrives everywhere and keeping it under control or even exterminating it in a sterile environment is at best difficult and at worst impossible. Stubborn biofilm contamination can resist cleaning/disinfection efforts with chemicals (cleaning in place – CIP), antibiotics, eddy current abrasion and heat (sterilisation-in-place – SIP). The presence of the biofilm contamination in pharmaceutical and biotechnical production systems threatens production flows, aseptic transfer and potentially might even affect the health of customers who use the products which come from the affected plant.
less
Biofilters more
​Are biologically active filters for cleaning various substances, e.g. through micro-organisms. They are often used in sewage treatment plants. Biologial filters break down substances into different components, depending on the micro-organism culture.
less
Bioreactor more
​Is the main area of interest in the biological production of substances. In a bioreactor, micro-organisms bring about intentional reactions or changes, depending on the purpose. A bioreactor is not only useful for production of a single procuct, but can produce several products through several stages and procedures.
less
Biotechnology more
​The integrated application of biochemistry, microbiology and process engineering with the aim of achieving the technical exploitation of the potential of micro-organisms, cell and tissue cultures. Biotechnology refers to the study of all methods with which life forms from single-cell organisms to highly developed animals are used for technical purposes. Some biotechnical methods are very, very old. Yoghurt and cheese were manufactured 3,200 years before Christ in the region now known as Iraq (Mesopotamia). Beer or yoghurt are just as much biotechnological products as genetically engineered Interferon.


less
Boundary layer fauna more
​Biological coating on surfaces by micro-organisms, e.g. bacteria and fungi
less
Bursting disc more
​Is a safety organ, which by bursting creates a greater pressure release cross-section in the event of excessive pressure, e.g. an explosion, and releases pressure into the atmospere in this way. The bursting disc is usually made of metal or graphite.
less
Bypass more
​A bypass is a diversion of the actual route so that various properties can be measured at places where measurement is not possible at the desired location.
less