This website uses cookies.

On our web pages and in our online shop, we use strictly necessary cookies and cookies that are needed to process your queries. We also use tracking cookies, which help us to optimize our online presence and offer you a better browsing experience as a result. ...

You can find further information in our Data Protection Statement. Data protection statement

Functional cookies

These cookies are strictly necessary to enable you to use all the functions and features of GEMÜ web pages. Consequently, they are enabled by default and cannot be disabled. If you wish to avoid these cookies, you can do so by changing the settings in your browser.

Web analysis cookies

Here you can decide whether you want to allow a unique web analysis cookie to be stored in your browser that will enable the website operator to record and analyse various statistical data. If you do not want to allow this, click on the following link to store the Piwik opt-out cookie in your browser.

Unfortunately, GEMÜ is currently unable to store settings for multiple browsers or about multiple user accounts. It is also possible that, irrespective of the security settings you have set in your browser, the cookies set by GEMÜ will be deleted when you close the browser and will therefore no longer be available in your next session. If you close or change your browser, or if you use more than one PC, you may have to make some of the changes again.

Precise temperature monitoring in systems and piping with new temperature sensor in the GEMÜ range

Precise temperature monitoring in systems and piping with new temperature sensor in the GEMÜ range

The new GEMÜ 3240 temperature transducer/switch now allows precise temperature monitoring in systems and piping across an even broader measuring range.

The GEMÜ 3240 temperature transducer/switch supersedes the existing GEMÜ 3220 product range with immediate effect. The new sensor's high-quality measuring cells are able to withstand media temperatures of between -40 °C and +150 °C and operating pressures of up to 160 bar while maintaining an accuracy of 0.35% FSO.
In addition to the considerably broader measuring scope, the new series scores highly in terms of its wide range of features. For demanding acid/alkali applications, all media wetted parts are available with PVDF encapsulation, for example.

IO-Link for intelligent networking
With an IO-Link interface, the GEMÜ 3240 temperature transducer/switch can be used centrally to automate and monitor processes. This is beneficial for system networking, for example, as it makes components compatible with one another and facilitates parameterization and data transmission.
The rotatable LED display is another advantage: The 4-digit display allows the current operating parameters to be viewed in any installation position.

Versatility
The new GEMÜ 3240 temperature transducer/switch can be used for a wide variety of applications. The sensor is a reliable temperature measurement and control instrument for use in cooling circuits or for monitoring sterilization processes. It is suitable for a huge variety of media, such as highly viscous or contaminated media. In addition, the high-quality material from which the sensor is made means that it is able to withstand even chemically corrosive media.

With its 3140-series pressure transducer/switch, which it launched back in 2018, GEMÜ has already been able to boast state-of-the-art measurement systems for measuring and controlling pressure. This device is now joined by the new temperature sensor, which broadens the scope of the measurement and control systems range.

 

Download

gb
.docx
75 K
idk
.jpg
512 K