This website uses cookies.

On our web pages and in our online shop, we use strictly necessary cookies and cookies that are needed to process your queries. We also use tracking cookies, which help us to optimize our online presence and offer you a better browsing experience as a result.

You can find further information in our Data Protection Statement. Data protection statement

Functional cookies

These cookies are strictly necessary to enable you to use all the functions and features of GEMÜ web pages. Consequently, they are enabled by default and cannot be disabled. If you wish to avoid these cookies, you can do so by changing the settings in your browser.

Web analysis cookies

Here you can decide whether you want to allow a unique web analysis cookie to be stored in your browser that will enable the website operator to record and analyse various statistical data. If you do not want to allow this, click on the following link to store the Piwik opt-out cookie in your browser.

Unfortunately, GEMÜ is currently unable to store settings for multiple browsers or about multiple user accounts. It is also possible that, irrespective of the security settings you have set in your browser, the cookies set by GEMÜ will be deleted when you close the browser and will therefore no longer be available in your next session. If you close or change your browser, or if you use more than one PC, you may have to make some of the changes again.

Focus on reliable and intelligent processes: GEMÜ CONEXO

Focus on reliable and intelligent processes: GEMÜ CONEXO

Video only available in German! GEMÜ focused entirely on the motto "Process reliability" at ACHEMA 2015. One example of this is CONEXO – the future of intelligent valve technology. This involves linking valve components which have an RFID chip to an IT infrastructure, comprising the CONEXO APP and the CONEXO Portal. Every valve and every relevant valve component, such as the body, actuator or diaphragm, can be clearly traced using serialization and read off at any time in the system using the RFID reader – the CONEXO PEN. The CONEXO APP, which can be installed on mobile devices, will not only simplify and improve the "Installation qualification" process; it will also make the maintenance process much more reliable and easier to document in the future. The app actively guides the maintenance technician through the maintenance schedule and directly provides him with all the information assigned to the valve, such as test reports, testing documentation and maintenance histories. This will optimize the maintenance processes in the systems and thus make a significant contribution to increasing process reliability. The film will provide an initial insight into the current project.