This website uses cookies.

On our web pages and in our online shop, we use strictly necessary cookies and cookies that are needed to process your queries. We also use tracking cookies, which help us to optimize our online presence and offer you a better browsing experience as a result. ...

You can find further information in our Data Protection Statement. Data protection statement

Functional cookies

These cookies are strictly necessary to enable you to use all the functions and features of GEMÜ web pages. Consequently, they are enabled by default and cannot be disabled. If you wish to avoid these cookies, you can do so by changing the settings in your browser.

Web analysis cookies

Here you can decide whether you want to allow a unique web analysis cookie to be stored in your browser that will enable the website operator to record and analyse various statistical data. If you do not want to allow this, click on the following link to store the Piwik opt-out cookie in your browser.

Unfortunately, GEMÜ is currently unable to store settings for multiple browsers or about multiple user accounts. It is also possible that, irrespective of the security settings you have set in your browser, the cookies set by GEMÜ will be deleted when you close the browser and will therefore no longer be available in your next session. If you close or change your browser, or if you use more than one PC, you may have to make some of the changes again.

IO-Link

1.0 and 1.1 use uniform standards

GEMÜ is also a driving force behind the development of sectors and technologies at a higher level. As such, GEMÜ developed the new communication standard IO-Link together with leading manufacturers of automation products and solutions. 

The first manufacturer of IO-Link devices for valve designs and process systems

GEMÜ is a founding member of the IO-Link consortium, which has developed a neutral, open interface that enables process, parameter and diagnostic data to be easily transmitted between control units (masters) and simple sensors and actuators (devices). With the redesign of the GEMÜ 1235 intelligent electrical position indicator and the development of the GEMÜ 4242 combi switchbox, GEMÜ is the first manufacturer of valve technology components provided with an IO-Link interface. This allows sensors and actuators to be controlled simultaneously, which enables the communication interface (based on a point-to-point connection) to transmit digital or analogue data as a serial telegram via a three-conductor connector.

Customer benefits

The IO-Link standard offers numerous benefits:

  • Additional information can be exchanged between the sensor/actuator and the control unit/guidance system down to the lowest field level. This information can be used for diagnostics and parameterization.
  • The use of IO-Link reduces the number of interfaces and assemblies required.
  • The system can be integrated easily into existing field bus systems and is simple to operate using standard engineering tools.
  • This integration does not require any changes to existing or usual topology and wiring (up to 20 m).
  • Procurement costs and installation time for screened cables and multi-pole parallel wiring will no longer apply in future, because all communication takes place over a standard M12 connector.

IO-Link has now been included as a standardized communication system in international standard IEC 61131-9.

Further information

Detailed information about the communication standard and the consortium, which has members such as Siemens, Beckhoff, B&R, Phoenix Contact, Pepperl+Fuchs, Tuck, IFM and Sick, can be found at www.io-link.com.

Software files for the IO-Link Master

PACTware 4 (without HART-Com DTM and help texts)

Turck software „IO-Link IODD Interpreter and DTM“

Turck software „DTM for USB IO-Link Master“

Configuration files

Downloads