GEMU's websites make use of cookies. If you are using the site, this means that you agree to the use of cookies. To implement personal settings, click here

Beer manufacturing / fermentation system

Beer manufacturing / fermentation system
Knowledge regarding beer brewing has existed for many thousands of years already and was even exercised by the ancient Egyptians using the simplest of means. Nowadays, the most modern of hygienic processes are used to manufacture highquality beer. When manufacturing beer, both the knowledge of the art of beer brewing and a whole host of machinery and materials are needed. Using various process steps, water, barley, hops and yeast are combined to make the drink which is supported by the German beer purity law. The soluble, filtered extract gained from the malt when mashing is heated. This hot wort is cooled down. The next important production step is fermentation. For this purpose, yeast and sterile air / oxygen is added to the cooled wort. The oxygen serves to activate the yeast cells. This green beer is piped into the fermentation tanks. The yeast attenuates the extract / sugar in alcohol and carbon dioxide, releasing heat.
more Applications

Useful for download

GB
pdf
157 KB
DE
pdf
147 KB
FR
pdf
141 KB