GEMU's websites make use of cookies. If you are using the site, this means that you agree to the use of cookies. To implement personal settings, click here

Continuous disinfection of cooling lubricants

Multi-port valve blocks: Continuous disinfection of cooling lubricants and cutting fluid
In the metalworking industry, cooling lubricants and cutting fluids are essential for machining processes to avoid any change in the structure of the tools and materials. In addition to water and oils, these also contain additives such as antifoaming agents, stabilizers, emulsifiers and anti-corrosion additives. To allow the cooling lubricants to be used for longer, they are treated and cleaned using methods such as filtration. After an extended period of use, water-soluble cooling lubricants often become tainted with bacteria or fungi, which results in a strong odour and also impairs the function of the cooling lubricant fl uid, among other problems. This also represents a signifi cant health risk for production staff.

Useful for download

.pdf-File
162 KB
DE
.pdf-File
161 KB
GB
more Applications