Measurement and control systems

Measurement and control systems

GEMÜ is a system provider that develops, manufactures and handles all measurement and control system components for complex processes. These components are available as plastic and stainless steel solutions.

Extensive product range

This variety, which extends to cover all areas of application, is unique to GEMÜ. At the same time the extensive product range offers a wide choice of combination options. The precision-adjusted components are ideal for processes of differing qualities built onto one another.

Appropriate control and measurement devices

Ensuring that production processes and plants always give full performance involves the ongoing capture, evaluation and processing of data. GEMÜ has developed the appropriate sensors and measurement systems for the process parameters of flow, pressure, temperature and levels. The electrical and optical position indicators display valve positions directly in the system. These displays may also be passed on to the higher-level control units. In conjunction with the valves, the positioners and process controllers form a functional unit that guarantees process stability.

Forcing automatization

GEMÜ is also a driving force behind the development of sectors and technologies at a higher level. Together with leading manufacturers of automation products and solutions, GEMÜ thus developed the new communication standard IO-Link. With this, sensors and actuators are controlled uniformly, something that was extremely difficult before. A serial communication interface based on a point-to-point connection will transmit digital or analogue data as a serial telegram. GEMÜ is a founder member of the IO Link Consortium, and the redesigned GEMÜ 1235 intelligent electrical position indicator has been fitted with an IO link interface. This makes GEMÜ the first IO link device manufacturer in the valve and process technology sector.