Q10 value
Más
QHD
Más
Qualified Hygienic Design (test system for cleanability of components)
Stage 1 includes the theoretical proof of hygienic construction. The compliance with these standards relevant for the respective component can be documented by an own certificate and a QHD mark stuck to the component. The manufacturer hereby declares that he has complied with the state-of-the-art with regard to the requirements for a hygienic construction specified in the regulations.
Stage 2 is verified by a standard test developed by the Faculty for Machine and Apparatus Study of the University of Munich, Freising – Weihenstephan. (practical proof of cleanability)
enos
Stage 1 includes the theoretical proof of hygienic construction. The compliance with these standards relevant for the respective component can be documented by an own certificate and a QHD mark stuck to the component. The manufacturer hereby declares that he has complied with the state-of-the-art with regard to the requirements for a hygienic construction specified in the regulations.
Stage 2 is verified by a standard test developed by the Faculty for Machine and Apparatus Study of the University of Munich, Freising – Weihenstephan. (practical proof of cleanability)
Qualification
Más
Quenching
Más
Recommended value
Más
Regulation
Más
Relative pressure
Más
Relief valve
Más
Resistance
Más
Reverse osmosis
Más
Reynolds figure
Más
Rinsing
Más
RO
Más
RoHS
Más
Roughness depth
Más
Roughness parameter
Más
Comparable measured values determined from the roughness profile of technical surfaces by stylus instruments
The following are distinguished according to DIN 4768 Section 2.3:
Mean roughness value Ra = arithmetic mean of the distances between the roughness profile and the middle line within the measuring distance.
Single roughness depth Zi = distance between two parallel lines which touch the roughness profile at the highest and lowest point in a single measuring distance and the middle line.
Averaged roughness depth Rz = arithmetic mean of the single roughness depths of five consecutive measuring distances.
Maximum roughness depth Rmax = greatest single roughness depth occurring on the total measuring line.
enos
The following are distinguished according to DIN 4768 Section 2.3:
Mean roughness value Ra = arithmetic mean of the distances between the roughness profile and the middle line within the measuring distance.
Single roughness depth Zi = distance between two parallel lines which touch the roughness profile at the highest and lowest point in a single measuring distance and the middle line.
Averaged roughness depth Rz = arithmetic mean of the single roughness depths of five consecutive measuring distances.
Maximum roughness depth Rmax = greatest single roughness depth occurring on the total measuring line.
Sanitation
Más
Sealing
Más
Self-draining
Más
A frequently misused term for the design and construction of a media-carrying component or plant section which enables the complete draining of a pipe system without outside intervention.
The term suggests fully automatic draining. Complete self-draining is not possible in reality, especially because the increased adhesion of a working medium leads to the medium sticking partly to the surfaces of the pipe sections, valves or vessels to be emptied. Actually the optimisation of a plant can merely ensure that a so-called unhindered outlet can take place. Ideally no media residue in the form of puddles or clogged material remains in the pipe. To counteract an increased media adhesion it may be useful to fit transverse pipes and components with an appropriate drop/gradient. This is also recommendable to overcome gravity and define an orderly outlet in direction and time. See also Free outlet and Optimum draining.
enos
The term suggests fully automatic draining. Complete self-draining is not possible in reality, especially because the increased adhesion of a working medium leads to the medium sticking partly to the surfaces of the pipe sections, valves or vessels to be emptied. Actually the optimisation of a plant can merely ensure that a so-called unhindered outlet can take place. Ideally no media residue in the form of puddles or clogged material remains in the pipe. To counteract an increased media adhesion it may be useful to fit transverse pipes and components with an appropriate drop/gradient. This is also recommendable to overcome gravity and define an orderly outlet in direction and time. See also Free outlet and Optimum draining.
Servo controlled
Más
The actuation, e.g. a valve actuator, does not control the sealing mechanism of a valve directly but with the aid of the operating pressure applied in the valve. The necessary forces are generated by defined areas and their exposure to the operating pressure. Small control bores and channels serve for this so that relatively high operating pressures can be handled by relatively small actuators (usually electromagnetic). Terms such as forced lift and auxiliary controlled are also used manufacturer-dependently. Servo controls are also familiar for example as steering and brake assistance in vehicles.
enos
Set value "w"
Más
Short-stroke
Más
Signals
Más
SIL
Más
SIP
Más
Smoothness
Más
Soiling
Más
Solenoid valve
Más
Spores
Más
Germ cells of micro-organisms which are also permanent forms in bacteria.
Permanent form of micro-organisms formed under unfavourable conditions which germinate in a favourable environment, reproduce and survive heating to 75 °C for 20 minutes. Bacteria spores have storage substances and solid, resistant cell walls.
enos
Permanent form of micro-organisms formed under unfavourable conditions which germinate in a favourable environment, reproduce and survive heating to 75 °C for 20 minutes. Bacteria spores have storage substances and solid, resistant cell walls.
Square-stroke
Más
Steam sterilisation
Más
Sterilisable
Más
Sterilising
Más
Sterility
Más
Sump space
Más
Surface
Más
There are three different types of surfaces:
Surface, geometric: An ideal surface the nominal shape of which is defined by the drawing and / or other technical documents. According to DIN 4760, sub-section 2.3.
Surface, actual: The approximate projection of the real surface of an element determined by measurement. According to DIN 4760, sub-section 2.2.
Surface, real: The surface which separates the object from the space surrounding it. According to DIN 4760, sub-section 2.1.
enos
Surface, geometric: An ideal surface the nominal shape of which is defined by the drawing and / or other technical documents. According to DIN 4760, sub-section 2.3.
Surface, actual: The approximate projection of the real surface of an element determined by measurement. According to DIN 4760, sub-section 2.2.
Surface, real: The surface which separates the object from the space surrounding it. According to DIN 4760, sub-section 2.1.
Surface colony count
Más
Surface treatment
Más