Glossario GEMÜ per valvole e

componenti per l'automazione

Glossario GEMÜ per valvole e

I-controller ulteriori informazioni
​Controllers in which there is a proportional relation between the control error and the positioning speed.
meno
IAMFES ulteriori informazioni
​International Association of Milk, Food and Environmental Sanitarians
meno
In-process inspection ulteriori informazioni
​Inspection during the process Inspections determined by the manufacturer which are conducted in the course of manufacture of the product.
meno
Increased safety ulteriori informazioni
​Increased Safety is the guarantee that measures have been developped for electrical equipment, so that they can even be used  in areas at risk of gas explosion.
meno
Inert gas ulteriori informazioni
​Inert gases are gases which are extremely neutral due to their chemical properties.
meno
Inertization ulteriori informazioni
​Inertization isthe exchange or conversion of a reactive gas into an inert gas.
meno
Infect ulteriori informazioni
​Transmission and penetration of foreign organisms (e.g. parasites, bacteria, fungi) or viruses into an organism or a closed system.
meno
Inlet distance ulteriori informazioni
​The inlet distance is the length of a pipe in the flow to a flowmeter.
meno
Instrument sensor ulteriori informazioni
​Is a sensor which continuously measures a non-electrical variable and alters its internal electrical value according to the measured value, e.g. pressure or temperature sensors.
meno
Interbus ulteriori informazioni
​Interbus is a bus system specially required for  industrial use. It is used to transmit information to a company via a cable. Like a fieldbus, the interbus is a a communication connection between actuators / sensors and their control units, yet unlike the fieldbus system, it offers other advantages, such as faster and easier commissioning.
meno
Intercrystalline corrosion ulteriori informazioni
​Intercrystalline corrosion refers to corrosion within specific corrosive agents along the crystal boundaries of metal crystals, while the grains (metal crystals) themselves are hardly affected. During this process, the grains can separate from the grain structure, causing the steel to lose its solidarity.
Intercrystalline corrosion in stainless steel is caused by the dispersion of chromium-rich carbides at the crystal boundaries, which causes chromium depletion in neighbouring zones. These chromium carbide dispersions are triggered by extreme heat in the critical temperature range of 500 – 800 °C. Chromium nickel steels with a higher carbon content are particularly susceptible. So-called low-carbon steels (with a carbon content of less than 0.03%) have a high resistance to intercrystalline corrosion.
meno
Intrinsic safety ulteriori informazioni
​See ATEX
meno
Ion exchanger ulteriori informazioni
​An ion exchanger replaces cations or anions in a medium through the addition of other equivalent cations or anions. This is used e. g. for softening water.
meno
IP protection class ulteriori informazioni
​Is the protection of electrical equipment through housings, flaps and covers in order to guarantee personal protection. IP protection classes are standardized and stipulated in DIN EN 60529 . The aim is to prevent the penetration of water and particles into electrical equipment.
meno
ISO ulteriori informazioni
​​International Standardization Organisation
meno
ISPE ulteriori informazioni
​International Society for Pharmaceutical Engineering
meno
JIS ulteriori informazioni
​Japanese Industrial Standard
meno
Joint ulteriori informazioni
The linking/joining together of multiple parts/substances using mechanical, chemical or physical means.
meno
KBE ulteriori informazioni
​Kolonien bildende Einheiten - Colony forming unitsSee also Colony number.
meno
Kv ulteriori informazioni
​(VDI/VDE 2173 and DIN-ISO-EN): Kv is the flow coefficient of a valve and is expressed by a number. It is defined under uniform conditions and therefore creates a possibility for comparison and the mathematical basis for calculation in a different operating situation. A flow constant rsulting from a pressure difference of ∆p 1 bar, a test temperature of the ambient atmosphere and the fluid between 5° C and 30° C (usually 20° C) and the uniform liquid test medium with a density of 1000 kg/m3 and a kinematic viscosity of 10 -6 m2/s (water H2O) guarantee a comparability of the valves at a common denominator. The measuring result is expressed by a number. This number is the characteristic number of the valve. If no unit of measure is assigned to the characteristic number, this means that the characteristic number refers to cubic metres per hour (m3/h). If the characteristic number refers to another unit of measure, this unit of measure must be assigned directly to the characteristic number (e.g. 3200 l/h) All valves can be tested at a pressure freely selected by th manufacturer. Only the difference of p1 bar between the inlet side (p1) and the outlet side (p2) is to be determined. The diaphragm vlave is an exception. In this functional principle the test must always take place at the maximum permissible operating pressure of the respective valve (diaphragm stretch). The opening state of the valve is any so that a characteristic can be determined, for example, over the whole stroke range depending on the valve position. Formulae serve to take into account all the parameters and physical variables deviating from the test. Since liquids, gases and steam are subject to different laws, different formulae also exist. The standardised calculation formulae are very extensive, therefore the "simplified" formulae are normally used. Here it is important that they cannot be fully abbreviated and the unit used respectively for the value Q or the Kv value is identical. (See also CV for American version of Kv).
meno
KV ulteriori informazioni
​The KV measured value: Value of a single valve in any opening position
meno
Kv 100 ulteriori informazioni
​the KV measured value of a single fully open valve
meno
KV test pressure for all other valves ulteriori informazioni
​​p1 frei wählbar - 1 bar = ∆ p 1 bar
meno
KV test pressure for diaphragm valves ulteriori informazioni
​p1 Betrieb max - 1 bar = ∆ p 1 bar
meno
Kv value ulteriori informazioni
​The Kv value is a standardized variable. It is the measured flow Q of water (5 to 30 °C) in m3/h with a pressure loss of 1 bar and the respective stroke. The Kvs value is the flow with a rated stroke of 100%.
meno
Kvs ulteriori informazioni
​The planned KV measured value for an identical series of fully open valves
meno