With the new, optimized Nexus Connect®* flare connection, the Ingelfingen-based technology company GEMÜ is now introducing an innovative flare connection for its CleanStar and iComLine valve series. As a result, GEMÜ is now offering its customers another optimized flare connection to GEMÜ valves and a range of suitable fittings.
In the semiconductor industry, flare connections have long been an established standard in the area of media distribution and media supply. However, this connection type reaches its limits in applications with extreme pressure and temperature requirements. GEMÜ now has an innovative solution. The Nexus Connect® connection not only provides greater safety, it also ensures seamless compatibility with existing fitting systems.
GEMÜ already offers the optimized flare connections that are currently available on the market for GEMÜ CleanStar and GEMÜ iComLine valves. With the Nexus Connect® connection, we now have the opportunity to offer this connection consistently throughout the entire HP product range and to supply suitable fittings for them.
Due to its compatibility with the most widespread optimized flare connection, GEMÜ's customers can equip their plants without needing to replace other components. This is also underlined by the successful test results of Fit-Line Global, which confirm that both connection types can be seamlessly combined.
The introduction of this Nexus Connect® includes the GEMÜ CleanStar valves series, which will initially be available with welded-on adapters as well as in the compact SpaceSaver version. For the iComLine series, the connection will also be available in a machined version on single valves as well as the GEMÜ PC50 valve blocks. Its expansion to the entire HP product range is planned.
With the Nexus Connect® connection, GEMÜ is setting a new standard with respect to flexibility and performance in the semiconductor industry. Integrating this innovative design not only promises to make installation easier, but also to increase efficiency and reliability in critical production environments.
Nexus Connect® is a registered trademark of Fit-Line Global